Emwin 5.50 6.10 Can not find GUITASK_SetMaxTask

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Emwin 5.50 6.10 Can not find GUITASK_SetMaxTask

445 Views
18222967901
Contributor I

When I see the emwin 5.50g had been updated on the www.nxp.com, i download it and replaced emwin 5.38 which in my project. I found that the project had an error "Error: L6218E: Undefined symbol GUITASK_SetMaxTask (referred from emwin_support.o)." All #define i had checked were open,I thought that the library had some problems,because the emwin 5.38 was 6.14MB,and emwin 5.50 was 4.2MB.

Today i find that emwin 6.10 had updated ,i downloaded it find that the same question.

Could you check it ?

Thanks and Best wishes.

Based on SDK RT1064 2.7.0

0 Kudos
1 Reply

372 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

Please refer to the other post and the last response provided.

https://community.nxp.com/thread/529662 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos