imx6ull secure-boot enabling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull secure-boot enabling

1,358 Views
jay_kaneria
Contributor I

Hi, 

I have enabled secure-boot option in defconfig of u-boot, signed image with appropriate certificates. Now, i am trying to flash the image on board using mfgtool. After flashing the image, when i check the hab_status, i am getting hab events.

Now when i flash the same signed image using "imx_usb_loader" like mentioned here "https://community.nxp.com/docs/DOC-94117 ", i am not getting any hab events in  'Serial Download Mode'. My signed u-boot image works properly in 'Serial Download Mode' but agains gives hab events when i switch the mode.

I am suspecting problem with my "ucl.xml" file in mfgtool. I am attaching the "ucl.xml" file here.

Labels (1)
0 Kudos
1 Reply

1,259 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jay

one can refer to

Secure Boot and HAB document for i.MX6ULL 

also additional document was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos