iMX6 Solo SABRE Smart Device - LInux Rocko Build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 Solo SABRE Smart Device - LInux Rocko Build

772 Views
pravinyadav
Contributor III
  • We are porting rocko build for iMX6 Solo SABRE Smart Device (iMX6SolosabreSD)
    BSP: fsl-bsp-relase rocko

    https://source.codeaurora.org/external/imx/meta-fsl-bsp-release/tree/imx/README?h=rocko-4.9.88-2.0.0...

    Problem observed - Failed to start x server

    MACHINE = imx6solosabresd
    DISTRO = fsl-imx-x11

    IMAGE = fsl-image-validation-imx


    failed to start X server


    X.Org X Server 1.19.3
    Release Date: 2017-03-15
    X Protocol Version 11, Revision 0
    Build Operating System: Linux 4.4.0-174-generic x86_64
    Current Operating System: Linux imx6solosabresd 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d61147 #6 SMP PREEMPT Wed Mar 18 14:24:33 IST 2020 armv7l
    Kernel command line: console=ttymxc0,115200 nosmp root=/dev/mmcblk3p2 rootwait rw
    Build Date: 14 March 2020 12:48:23PM

    Current version of pixman: 0.34.0
    Before reporting problems, check http://wiki.x.org
    to make sure that you have the latest version.
    Markers: (--) probed, (**) from config file, (==) default setting,
    (++) from command line, (!!) notice, (II) informational,
    (WW) warning, (EE) error, (NI) not implemented, (??) unknown.
    (==) Log file: "/var/log/Xorg.0.log", Time: Sat Mar 14 04:37:49 2020
    (==) Using config file: "/etc/X11/xorg.conf"
    (==) Using system config directory "/usr/share/X11/xorg.conf.d"
    [ 1] Failed to open device: No such file or directory, Try again...
    [ 2] Failed to open device: No such file or directory, Try again...
    [ 3] Failed to open device: No such file or directory, Try again...
    [ 4] Failed to open device: No such file or directory, Try again...
    [ 5] _OpenDevice(1229): FATAL: Failed to open device, errno=No such file or directory.
    xinit: giving up
    xinit: unable to connect to X server: Connection refused
    xinit: server error

Labels (4)
0 Kudos
1 Reply

631 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

https://community.nxp.com/message/1086549 this will do help for you.

0 Kudos