Hi,everyone
I want to use the imx7solo to control BLDC without sensors. And I have read the reference manual of imx7solo. About the FTM, I have some question:
1. Which onchip module will receive the output trigger of the FTM? I can't find any information about this.
2. Which signals are the hardware synchronization source? The RM has referred to TRIG0/1/2, I cannot see any information about these trigger source.
3. Can I use the FTM of imx7solo to control BLDC without sensors? The imx7solo has no PDB module. How can I synchronzie the ADC and FTM?
Hi daqin
I am afraid such ftm imx7solo examples are not available, sorry. Since ftm module
is the same may be useful to look at below documents:
https://www.nxp.com/docs/en/application-note/AN5303.pdf
https://www.nxp.com/docs/en/supporting-information/Flex-Timer.pdf
Need sample code of FTM for PWM Generation
linux/pwm-fsl-ftm.c at master · torvalds/linux · GitHub
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------