AnsweredAssumed Answered

About S12Z ADC sample time and interrupt

Question asked by xue j on Mar 13, 2020
Latest reply on Mar 15, 2020 by Daniel Martynek

1.ADC saple time

the above figure as the example ,8-bit data,4 cycle sampling , the adc min sampling time=?

the adc sampling time =adc clock/12 or 13? if is 13,why? 

2.ADC Interrupt

If I want trigger the adc interrupt by timer0,every 50ms sample the data 100times by AN3,how to do it ?

The INTFLG[3:0] is to configure the interrupt flag number(1~15),the interrupt flag number is defined by myself? If I want to sample the AN3,can I set the interrupe flag number is 1 or 2,...?

Outcomes