Hi,
I asked a question to use u-boot command to install u-boot-nand.imx to NAND rather than run kobs-ng from zImage-initramfs on iMX6ull, the anwser was not possible, we have to run kobs-ng ramdisk to install u-boot-nand.imx to NAND. So I have to build Yocto Linux ramdisk image to include kobs-ng, I have also heard that Linux ramdisk image need to use imx-kobs.dtb, any document or instruction to build Yocto Linux ramdisk with kobs-ng and device tree imx-kobs.dtb?
Thank you.
Kind regards,
- jupiter
Hi jupiter
one can look at
https://community.nxp.com/thread/477997
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Thanks for the clue, I've built the kobs-ng in ramdisk, but how can I set up imx6ulz-kobs.dtb for using by kobs-ng and ROM?