MK36A FlexCan only 125k Baud

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK36A FlexCan only 125k Baud

Jump to solution
900 Views
lukas_berger
Contributor II

Hello,

i am running the flexcan_interupt example program from the FRDM-KW36 Dev. Board on the MKW36A512VFP4.

The example runs fine with a baud rate of 125k. But with all other standard baud rates like 100k, 250k, 500k or 1000k. I can't get the example to work. With a baud rate of 125k I can see the Send Message clear on the Scope but with all the other I can't get a clear Message to work. Is there something I have to change at the Clock or bit time timings?

The strange thing I don't understand is that the example is configured standard with 1000k baud rate.

Every advice is highly appreciated.

Regards,

Lukas

Tags (3)
1 Solution
848 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Could you please help me checking this thread and confirm if this helps you ?

[KW36] FlexCAN Bit Timing Parameters Setup 

I believe that you can find there the information you are looking for.

Regards,
Estephania

View solution in original post

1 Reply
849 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Could you please help me checking this thread and confirm if this helps you ?

[KW36] FlexCAN Bit Timing Parameters Setup 

I believe that you can find there the information you are looking for.

Regards,
Estephania