Hi
in meanwhile I got a copy of the can bootlader form NXP support.
I tried to run it and I get this issue:
Exception in thread "main" java.lang.UnsatisfiedLinkError: C:\Users\xyz\Desktop\vector_support\S32K148_Bootloader\S32K148_Bootloader\Bootloader interface\Java interface\win32com.dll: Can't load IA 32-bit .dll on a AMD 64-bit platform
Will installing 32 bit java solve the issue?
Yes, installing the 32bit version seems to help.
Hello Jiri,
I am having same issue. Can you please help me with this ?
I am using AN12218SW Sample application got from below link
Can I get win32com.dll for 64 bit platform ?
Please revert.
Regards,
Akshay K.
Hi,
If I'm correct - win32com.dll is part of Java installation - Java Communication API and is already present in serial bootloader interface root. From readme.txt I can see that this interface requires Java jre7:
To open this interface:
1.- Double click on Serial_Bootloader_Interface.jar
2.- or In cmd you can use the following:
c:\your_directory\your folder\Java interface>java -jar Serial_Bootloader_interface.jar
3.- or select open with and chose the javaw.exe file from your installed Java run time environment, for instance:
C:\Program Files\Java\jre7\bin\javaw.exe
To use the Bootloader interface simply:
1. Select communication port
2. Select baudrate, the default baudrate is 19200.
3. Select SREC file to send
4. Click download, and the SREC file will be sent line after line.
I can use this interface without any issue on 64bit win10:
Jiri
Hi,
what Bootloader and version do you have?
Jiri