iMXRT1021 blowing efuse via executable code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1021 blowing efuse via executable code?

Jump to solution
1,162 Views
t_thurgood
Contributor III

Hi,

We are using the iMXRT1021 and need to blow efuses via executable code.

I have looked at IMXRT1020RM.pdf, but this describes efuse functionality, but not usability. At the moment we can blow efuses either using Blhost/flashloader or MCU Boot Utility/Flashloader.

Is there an application note explaining internal efuse programming?

Can anyone advise how to do this?

I have found a reference to EFUSE_PROG_SUPPLY_GATE which I assume needs to be set, then what?

br,

Tony

1 Solution
1,078 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Tony Thurgood,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to suggest you refer to the ocotp demo which is from the SDK library, this demo demonstrates that uses the KSDK software to access eFuse map.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
1,078 Views
carstengroen
Senior Contributor II

Tony,

perhaps this can be of some help: https://community.nxp.com/thread/492451 

(I assume the same procedure for the 102x ?!)

1,078 Views
t_thurgood
Contributor III

Hi Carsten,

Thanks for the link.

I think that is all useful information to get this working for me.

br,

Tony

1,079 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Tony Thurgood,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to suggest you refer to the ocotp demo which is from the SDK library, this demo demonstrates that uses the KSDK software to access eFuse map.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,078 Views
t_thurgood
Contributor III

Hi Jeremy,

Thanks for the info.

best regards,

Tony

0 Kudos