i.MX6ULL GPMI NAND Flash driver example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL GPMI NAND Flash driver example

894 Views
jlin
Contributor I

Hi,

Is there a i.MX6ULL GPMI NAND Flash driver example? I did not find that in the SDK, probably because the EVK have NAND Flash as optional only (not populated by default).

Tags (1)
0 Kudos
1 Reply

794 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

one can look at

How-To use NAND boot on i.MX6UL EVK board 

https://community.nxp.com/thread/517143 

rt-thread/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/gpmi at master · RT-Thread/rt-thread · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos