Does i.MX8M support boot from QSPI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX8M support boot from QSPI?

Jump to solution
1,423 Views
m_c
Senior Contributor I

In i.MX8M reference manual revision 1.

1.6 says support boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet.

pastedImage_2.png

6.1 says support boot from SD/MMC and NAND flash.

pastedImage_1.png

Which one is right?

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,129 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello m.c.

Both are rigth the i.MX8M can boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet, but the boot ROM suport NAND and SD/MMC, The boot ROM uses the state of the BOOT_MODE and eFUSEs to determine the boot
device. For development purposes, the eFUSEs used to determine the boot device may be overridden using the GPIO pin inputs.

Regards

View solution in original post

0 Kudos
2 Replies
1,130 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello m.c.

Both are rigth the i.MX8M can boot from NAND, SDIO/MMC/SDXC, eMMC, SPI, USB, QSPI and Ethernet, but the boot ROM suport NAND and SD/MMC, The boot ROM uses the state of the BOOT_MODE and eFUSEs to determine the boot
device. For development purposes, the eFUSEs used to determine the boot device may be overridden using the GPIO pin inputs.

Regards

0 Kudos
1,129 Views
juergene
Contributor III

Hi Bio_TICFSL,

i don't get it. 

This thread (https://community.nxp.com/thread/473293) is saying that there is no boot options from QSPI.

So how do i implement booting from QSPI after your statement.

Thanks in advance!

Best regards,

Juergen

#i.mx8m

0 Kudos