I want to generate LIN driver code for MC9S12ZVL32F0CLF but when I verify NPF file then I am getting
Description Resource Path Location Type
line: 456 "DG8" - The N_Cr_timeout is a property of LIN 2.1 slave nodes only. LIN2_2019.ldf /LIN_DriverCreation/Sources line 456 Problem
For LDF file there is no issue.
Thank you in advance.
Hello Chaitanya,
I'm very sorry for the delay. I recommend you to look at the LIN specification. There you can find more details about N_Cr_timeout.
https://www.cs-group.de/wp-content/uploads/2016/11/LIN_Specification_Package_2.2A.pdf
Did you follow the information in the error that the N_Cr_timeout is a property of LIN 2.1 slave nodes only?
Also, the AN5122 and attached Eclipse User Manual can be useful.
https://www.nxp.com/docs/en/application-note/AN5122.pdf
Some examples can be found in the LIN driver installation folder.
https://www.nxp.com/webapp/Download?colCode=FSL_LIN_2.X_DRIVER
I hope it helps.
Best Regards,
Diana
Thank you for your response. I got new LDF and now don't have that error.
but while Flashing the program into DEVKIT-ZVL128 getting CRC Error that you can find in below screenshot.
I am getting error only when using processor expert generated code. For without processor expert mode there is no error but I need to use processor expert mode.
I added sample code with processor expert in the attachment.
I am new for LIN and working on urgent project so quick response is appreciated.
Hello Chaitanya,
It seems that there is a conflict with the generated code. I have found a similar issue in the community with the solution.
Please, look at this link:
https://community.nxp.com/message/971435
I believe it helps you.
Best Regards,
Diana
Yes you are right. Problem is due to conflict with generated code.
I modified map file and checked still having ISR redefinition error and added text automatically removing when I clean and build it.
https://community.nxp.com/message/1239752 here I added same problem and my sample file. Can please check from you side and let me know.