Which Vivante VDK version I can use it on imx6Q with Yocto 2.4(rocko)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which Vivante VDK version I can use it on imx6Q with Yocto 2.4(rocko)

970 Views
zohanlin
Contributor IV

Dear all,

My OS is Yocto 2.4(rocko), and the kernel version is 4.9.88.

The OS runs on IMX6Q.

I want to test Vivante GPU on IMX6Q, so I need Vivante VDK.

And I found the website i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release 

But the version seems to be out of date.

Could anyone tell me where I can download the VDK which is suitable for Yocto 2.4(rocko)?

Thanks,

zohan

Labels (4)
Tags (3)
0 Kudos
1 Reply

864 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Zohan,

The VDK is included in yocto, you don´t need to install them, if you are looking for the VTK please download at https://www.nxp.com/webapp/Download?colCode=VivanteVTK-v6.2.4.p4.1.7.8&appType=license 

Regards

0 Kudos