i.mx6dl sabre 1920x720 lvds display.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6dl sabre 1920x720 lvds display.

578 Views
samet_kocatepe
Contributor I

Hi community,

Currently i'm working with i.mx6 sabredl development board. i followed nxp document IMXLXYOCTOUG and achieved to bootup with sd card. Board works well with default hannstar 10.1" . Now, i m  trying to connect and operate 1920x720 LVDS display (datasheet is attached) with the sabre board. As i saw from schmatic files and datasheet of the display, i will need converter board to convert from 30pin LVDS to 60 pin LVDS (i will make the converter board). 

So,it will be really appreciated to point me that which configurations i should  make on yocto to work 1920x720 mitsubishi display ? 

Thanks.

Samet 

Labels (1)
Tags (2)
0 Kudos
1 Reply

451 Views
igorpadykov
NXP Employee
NXP Employee

Hi samet

for new lvds lcd settings one can check:

imx6q and lvds. 

https://community.nxp.com/thread/355690 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos