Does MKV31F256xxx12 sdk support Peripherals Config Tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MKV31F256xxx12 sdk support Peripherals Config Tool?

Jump to solution
1,176 Views
dthompson
Contributor II

MCUXpresso IDE v11.0.1 [Build 2563] [2019-09-01]

SDK_2.6.0_MKV31Fyyyxxx12.zip

where yyy is either 512 or 256.

both sdk's are version 228 2019-06-14

both sdk's are manifest 3.5.0

The 256 processor variant produces the following warning/error when the Peripherals Config tool is selected:

Device Configuration tool does not support selected processor. Select different tool.

The 512 variant did not exhibit the problem. Partial screen shot attached. Please advise on how to remedy this.

Tags (1)
1 Solution
923 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi David,

 

Unfortunately, this device is not supported by the Peripherals Config Tool. You can check which devices are supported by the MCUXpresso Tools in the following link.

 

https://community.nxp.com/docs/DOC-333073 

 

Hope it helps!

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
923 Views
Lukas_Heczko
NXP Employee
NXP Employee

Hi David, 

good news is that MKV31F256xxx12 will be supported by Peripherals tool in MCUXpresso Config Tools v7 released at the end if this year.

Regards,

Lukas

923 Views
dthompson
Contributor II

Excellent. Thank you for the timely reply and clarity.

0 Kudos
924 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi David,

 

Unfortunately, this device is not supported by the Peripherals Config Tool. You can check which devices are supported by the MCUXpresso Tools in the following link.

 

https://community.nxp.com/docs/DOC-333073 

 

Hope it helps!

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos