IMX6Q PCIE BAR and MSI-X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q PCIE BAR and MSI-X

594 Views
liyongzhi
Contributor I

Hi Sir

   I have two question to confirm.

   1. Is IMX6Q PCIE supporting MSI-X interrupt ? If yes,how many interrupt it supports?

   2. How many PCIE BAR IMX6Q supports? And the size of each BAR.

 

Thanks

Tags (1)
0 Kudos
1 Reply

508 Views
igorpadykov
NXP Employee
NXP Employee

Hi yong

MSI-X is supported acording to Table 48-2. Core Interface Summary i.MX6DQ Reference Manual,

for bar details one can check

Driver access PCIE Device via IO port failed with IMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos