CMSIS-DAP and JLINK debuggers no longer working on IMXRT1050EVKB board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMSIS-DAP and JLINK debuggers no longer working on IMXRT1050EVKB board

Jump to solution
2,143 Views
scottlarson
Contributor II

Hi,

After a few days of debugging on my iMX1050EVKB board, CMSIS-DAP no longer recognizes that there is any processor there, nor does a JLINK debugger. I've also tried IAR tools and they don't recognize it either. Is there any test I can run to see if the processor is fried or something else is wrong with the board or debugger?

Here is output from IAR:

Fri Oct 18, 2019 18:03:47: Loading the CMSIS-DAP driver
Fri Oct 18, 2019 18:03:47: Probe: CMSIS-DAP probe SW module ver 1.17
Fri Oct 18, 2019 18:03:47: Probe: Connecting to CMSIS-DAP:0227000047784e45003e9004d745004dddb1000097969900 firmware v.1.10
Fri Oct 18, 2019 18:03:47: Emulation layer version 4.48
Fri Oct 18, 2019 18:03:47: Notification to init-after-power-up hookup.
Fri Oct 18, 2019 18:03:47: Notification to core-connect hookup.
Fri Oct 18, 2019 18:03:47: CoreSight error: Cannot read IDCODE. No SWD access. Debugging is not possible.
Fri Oct 18, 2019 18:03:47: CPU status FAILED
Fri Oct 18, 2019 18:03:47: Cannot initialize DAP access.Connected DAP v1 on SWD. Detected IDCODE=0xbd11477.
Fri Oct 18, 2019 18:03:47: CoreSight error: Cannot read DP STAT register. No DAP access. Debugging is not possible.
Fri Oct 18, 2019 18:03:47: LowLevelReset(system, delay 200)
Fri Oct 18, 2019 18:03:50: Fatal error: Failed to connect to CPU   Session aborted!

Thanks,

Scott

0 Kudos
1 Solution
1,854 Views
converse
Senior Contributor V
1 Reply
1,855 Views
converse
Senior Contributor V