Hi,
I´m trying to load a u-boot image in an iMXRT1052 using uuu.
I´ve managed to include the RT105X family into uuu's "known processors". However, I get some libusb related errors when I plug the SoC in Serial Download mode:
Any advice on this? I´m using a virtual machine with Ubuntu 16.04. Can anybody help me checking if it works in a native Ubuntu machine?
Why there is no support for iMXRT105X family in uuu?
Thanks and regards,
Juanjo
Hi Juan Jose Vicente
Unfortunately, as you mentioned, RT10xx device family is not supported in the uuu tool, and at the moment there isn't plan to add the support, you can use mfgtool and elftosb tools. You can also check the community post:
One-stop secure boot tool: NXP-MCUBootUtility is upgraded to v1.4.0
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------