Hi ,
I am working on K64FN controller with KDS 3.2.0. I would like to detect low voltage on K64 for writing data to flash to protect it from being erase on power on reset. I am using processor expert for my project. I have tried the below configuration from link
Also I have made changes in unhandled vector from Build option of the CPU component to Own handler for every, so that I can check if LVD interrupt occurred. I did debug this by using J-link debugger. When I decreased the voltage below 3.1 V, it is showing me message that No source available at 0x00 and it is not going to the LVD_ISR.
My question is how to get the LVD interrupt fire in my code?
Any help is appreciated.
Thank you,
Kirti
Dear Kirti,
Only to confirm the debugger is not working correctly, could you toggle a pin or do something visible in the interruption and run your code without the debugger?
Best Regards,
Alexis Andalon
Hello Alexis,
Thank you for the reply.
Yes, the debugger is working fine. I have toggled the pin in interrupt and it worked for me. The problem was, I could not link the LVD handler function in the vector table. That's why the interrupt did not fire. I found out the component in processor expert to add the user interrupt. By using this component I could add the user interrupt to vector table.
I have followed below link to use the PE component.
Tutorial: User Interrupts with Processor Expert | MCU on Eclipse
Thanks again for the help.
Kirti
Hi Kirti,
Thanks for sharing you solution. I'm glad that you could solve your issue.
Best Regards,
Alexis Andalon