1.My quetion:JN 5169 Coordinator hang up when Roter joining the newwork.When the chip hang up ,there is no uart signal,no RF signal,and watchdog not reboot the device.When I reboot the device 2 days later, the problem disappear.
2.My envirorment:
1) SDK:JN-SW-4170 v1840
2)Coordinator:Base on JN-AN-1216-Zigbee-3-0-IoT-ControlBridge-v1011, we modify code about Uart1,RF signal handle,table size, etc.
3)the router is zigbee test tool, not real device.
3.My Operational steps:
1)Coordinator form the network
2) join other router in to the network
3) when the chip han up, there has joined 20 nodes.
4.The problem is similar to Chip JN5169 hanging in Runing
5.The Coordinator Table Size:(we want to support 30 child nodes only)
Maximun Number of Nodes 30
Mac Table Size 35
Active Neighbour Table Size 35
Address Map Table Size 35
Broadcast Transaction Table Size 9
Child Table Size 35
Discovery Neighbour Table Size 8
Nwk Fc Save Count Bit Shift 10
Route Discovery Table Size 3
Route Record Table Size 1
Routing Table Size 60
6.when problem occur, there was no any ERROR in the uart log
7.The siffer log "5169hangUpLog.cubx"was attached below,(channel 11, panid 0x22DF) line 15469 was the last packet that coordinator sended.
8.How to find the root cause of the problem and solve it?
Hi Wei,
What is the error that you are seeing after the JN device? Could you please share your terminal log?
https://www.nxp.com/docs/en/data-sheet/JN5169.pdf 9.5 Interrupt system
Regards,
Mario
Hi WEI,
How do you know that the watchdog was activated?
Are you working with the ZGWUI?
What is the message that you see in the debug port?
Regards,
Mario
Hi Mario,
Thank you for taking the time to help me analyze the problem.
We had tested the watchdog before, it was activated and work fine.
We did't work with the ZGWUI, we work with our gateway in fact.
When this problem occured,all terminal log was in the "JN5169HangUp.txt" log, and the sniffer log"5169HangUpLog.cubx" was attached below.
Look forward to your reply.
Regards,
wei
Hi Wei,
After looking at the sniffer log, it seems like the radio is still alive as there is MAC Ack activity from the coordinator until packet 15552... "Network Status: Many-to-one Route Failure".
I am not sure if you have a blocking code in your application and that is the reason for a few time the radio is active.
Could you please increase the Broadcast Transaction table size?
Regards,
Mario
Hi Mario,
May be the coordinator was hang up until packet 15552.
I check the application code this morning, there is no blocking code, I will check it again to confirm that.
Is that the Broadcast Transaction table size cause this problem? How many changes are appropriate?
Regards,
Wei
Hi Wei,
Please look at the Broadcast Transaction table size.
Size of broadcast transaction table. The broadcast transaction table stores the broadcast transaction records, which are records of the broadcast messages received by the node.
https://www.nxp.com/docs/en/user-guide/JN-UG-3048.pdf
Your table size is equal to 9.
Regards,
Mario
Hi Mario,
I am checking the Broadcast Transaction table size and try to increase it.
Thank you for your advice!
Regards,
Wei