Change Led state from Coordiator - JN516x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change Led state from Coordiator - JN516x

1,437 Views
minhtan_uet
Contributor III

Hi Support team!
I use JN-AN-1216-Zigbee-3-0-IoT-ControlBridge as a coordiator to control Led from End device (Just change DIO state)
Is there have any Example for that?
Thanks :smileygrin:

Labels (3)
Tags (2)
0 Kudos
8 Replies

1,132 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Trian,

Did you try the ON OFF cluster option?

pastedImage_1.png

Regards,

Mario

0 Kudos

1,132 Views
minhtan_uet
Contributor III

Dear Mario Ignacio Castaneda Lopez Employé

As i know in the JN-SW-4170  have a lib for change led state base on PWM output. (LightingBoard.c, OnOffCommandHandler.c)
Actually. I need change state of some LED IO (>4 leds), As I understand , in the JN-AN-1218-Zigbee-3-0-Light-Bulb DimmableLight have create endpointpastedImage_5.png  pastedImage_1.png

to control led pin DIO13 with PWM

=>> How to create or add endpoint to control 4 leds? It so hard for me :smileysad:

If you have any idea for that, Please let me know.!

Thanks

0 Kudos

1,132 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Tran,

If you want to control 4 DIO. You have to set the direction of those pins.

Look at the LightingBoard.c file C:\NXP\bstudio_nxp\sdk\JN-SW-4170\Platform\DK4\Source\LightingBoard.c

The file is setting the PWM for the DIO13, You could take as reference. Also, look at the App_DimmableLight.c that provides a switch for the commands that you will receive.

Note: Be sure that the 4 pins support the PWM functionality.

Regards,

Mario

0 Kudos

1,132 Views
minhtan_uet
Contributor III

Dear Mario
Thannk for your response.
Relate to : https://community.nxp.com/message/1145323
I think to change state of leds (>1 led) have to adding new endpoint for each led ===>> It is correct?
So. How to add multi endpoint? or have any example?  Thanks a lot! :smileygrin:

0 Kudos

1,132 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Tran,

I think to change the state of LEDs (>1 led) have to add a new endpoint for each led ===>> It is correct?

It will depend on your application, if you want an endpoint for 4 LEDs, you could do it.

You could create endpoints for each LED.

Create new endpoints in the zpscfg file

pastedImage_4.png

1.6 Compile-Time Options ZigBee 3.0 Devices User Guide

You can follow the next link. https://community.nxp.com/docs/DOC-340508, the first section is for the kw41 but please look at the Router/zcl_options.h section.

Comment the next code app_zcl_task.c

            /*else if(E_ZCL_RESTORE_DEFAULT_REPORT_CONFIGURATION == psEvent->eZCL_Status)
            {

                vRestoreDefaultRecord(app_u8GetDeviceEndpoint(),
                                psEvent->psClusterInstance->psClusterDefinition->u16ClusterEnum,
                                psAttributeReportingRecord);
            }*/

You could send an active request and the router device, in this case, will response with the active endpoints.

Please let me know if you have any question.

Regards,

Mario

0 Kudos

1,132 Views
minhtan_uet
Contributor III

Dear Mario.
Hope you help!
pastedImage_1.png

PUBLIC void APP_taskRouter(void)

pastedImage_2.png

pastedImage_3.png
I have added 4 endpoint to control leds. It work well 
=> How to send response from Router to Coordinator when User press to button? (change state of sBaseDevice)
As i know, In the JN-AN-1220 There is already an AN that implements attribute reporting. Now i'm try to get information from it.
Can you give me an idea? 


Addition
For change state led with Group. I add some groups with same endpoint ( 4 group with same endpoint 1,2,3,4)

pastedImage_5.png

It work well when i send : pastedImage_6.png
Then, If i set all endpoints (8 endpoint - 2 Node) into one Group, It's false (# Destination Endpoint)
=> How to change state all led in the same time?
Can you give me an idea? 
Thanks you! :smileygrin:

0 Kudos

1,132 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Tran,

=> How to send a response from Router to Coordinator when User press to button? 

Depending on the cluster client/server that you previously set.

=> How to change state all led in the same time?

This is part of the application, you could create an endpoint with all the leds, or sending en endpoint broadcast.

Regards,

Mario

0 Kudos

1,132 Views
minhtan_uet
Contributor III

Dear Mario
Thanks a million for your help! 3000
It help me a lot. :smileygrin::smileygrin::smileygrin:

0 Kudos