iMX6q pcie rc and ep mode work together

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6q pcie rc and ep mode work together

765 Views
371554161
Contributor I

Now my pcie rc mode is working fine, it can enumerate an ep device(pcie to uart xr17v35x) properly.The software is imx6_platform_sdk_v1.1.0 (NO OS)

promblem:

(1)I would like to use Two i. mx6q boards, one is used as PCIe RC. The other one is used as PCIe EP,As shown in the photo below  

2013-04-07_15-43-46_818_small (1).jpg      My test routine is based on imx6_platform_sdk_v1.1.0, only pcie_test_rc.c, and I need an ep routine. Can you help me provide a pcie_test_ep.c routine, preferably based on imx6_platform_sdk_v1.1.0 (NO OS), or other routines and materials, I will be very grateful to you! My email address is 371554161@qq.com.

Best Regards
yong luo.

0 Kudos
1 Reply

567 Views
igorpadykov
NXP Employee
NXP Employee

Hi yong

I am not aware of baremeta or platform_sdkl pcie ep examples, however

one can look at patches provided on

i.MX6Q PCIe EP/RC Validation System 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos