Hi,
I would like to enable the interrupt for particular GPIO pin. I want ISR to get triggered when there is change in value on particular GPIO pin.
For example, how can I trigger ISR for below GPIO pin ? Also guide me what changes are required in below pin mux settings?
Thanks
Mohan
Hi Mohan,
select pin functionality ...
then within a code enable interrupt for PORTE
INT_SYS_EnableIRQ(PORTE_IRQn);
and add interrupt handler code
void PORTE_IRQHandler(void)
{
PINS_DRV_ClearPinIntFlagCmd(PORTE, 16);
PINS_DRV_TogglePins(PTD, (1<<16));
}
BR,
Petr