DS90UB914A-Q1/913 camera capture image problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DS90UB914A-Q1/913 camera capture image problem

719 Views
857849964
Contributor I

i am using DS90UB914A-Q1/913 camera to capture image

i can receive 913 camera data and save those,but the image is green. like below:

the 913 camera format is ccir601 8bit (UYVY),1280*720.

the CSI0 Sensor Configuration Register value: CSI_SENS_CONF = 0x00009A00 (External VSYNC mode ,UYVY , 10BIT_DATA_WIDTH,Sensor Protocol:Gated clock mode)

any idea about dealing with this problem?

thank a lot!

Labels (3)
0 Kudos
2 Replies

554 Views
igorpadykov
NXP Employee
NXP Employee

Hi lin

one can try to reuse adv7180 driver an check below

https://community.nxp.com/docs/DOC-332679 

ADV7181 on IMX6Q board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

554 Views
857849964
Contributor I

The issue was done!The data pin must to connect data 12 -19,if using yuv 8bit format camera!

0 Kudos