SPC5606 Spread function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5606 Spread function

1,238 Views
hansonhe
NXP Employee
NXP Employee

Customers are now doing EMC experiments in the laboratory. When testing at 320MHZ and 448MHZ frequency points, there will be a situation of exceeding the standard. At present, the main frequency of SPC5606 runs at 64MHZ.

Whether SPC5606S has Spread Spectrum function or not, see the data manual should be Freq Modulation module, that is Modulation Register. How to configure the specific guidance, whether there is a reference code, thank you.

0 Kudos
1 Reply

1,154 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I have posted example with calculations here:

https://community.nxp.com/docs/DOC-332383

The code is compatible with SPC5606S,

regards,

Peter

0 Kudos