Questions about receiving various CAN Msgs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about receiving various CAN Msgs

651 Views
jm_shin
Contributor I

Hello

We are considering using multiple MAILBOXs to handle the received Multi CAN Msg.
However, the test result shows that MAILBOX (0,1) with maximum 2ea including Tx/Rx can be used and 'STATUS_CAN_BUFF_OUT_OF_RANGE' is generated when using more than this.
ex)
#define RX_BUFF_IDX 0U, #define TX_BUFF_IDX 1U - ok
#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U - ok
#define RX_BUFF_IDX 0U, #define RX_BUFF_IDX_2 1U, #define RX_BUFF_IDX_3 2U - fail

How can I receive various CAN Msgs?
I was refer to example code of can_pal_s32k144

Thanks

Labels (1)
Tags (1)
0 Kudos
1 Reply

527 Views
PetrS
NXP TechSupport
NXP TechSupport
0 Kudos