Hi ,
when I use one qt demo to play multimedia on imx8qm, below is the bug printf,anyone can help me?
Using Wayland-EGL
FT_New_Face failed with index 0 : 1
Using the 'xdg-shell-v6' shell integration
====== AIUR: 4.4.5 build on May 20 2019 10:17:54. ======
Core: AVI_PARSER_03.06.06 build on Feb 25 2019 02:36:36
file: /usr/lib/imx-mm/parser/lib_avi_parser_arm_elinux.so.3.1
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:06.973633000
Language: und
Mime:
video/mpeg, systemstream=(boolean)false, parsed=(boolean)true, mpegversi
on=(int)4, width=(int)720, height=(int)720, framerate=(fraction)30000/1001, code
c_data=(buffer)000001b001000001b58913000001000000012000c48d8ba98516845a146300000
1b24c61766335372e3130322e313030
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:07.000816000
Language: und
Mime:
audio/mpeg, mpegversion=(int)1, channels=(int)2, rate=(int)44100, bitrat
e=(int)0
------------------------
[ 375.432372] [VPU Decoder] firmware version is 1.3.1
====== BEEP: 4.4.5 build on May 20 2019 10:18:00. ======
Core: MP3 decoder Wrapper build on Jan 11 2018 10:20:25
file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm_elinux.so.3
CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.01_ARMV8 build on Jan 11 2018 10:05:45.
===!!! Current pulsesink device is auto_null !!!===
[ 380.777560] [VPU Decoder] warn: wait_event_interruptible_timeout wait 5s
timeout
Hi igorpadykov,
Thanks.Gstreamer is already included, for I can use gplay command to play video below.But when I use qml mediaplayer to play video, it failed.
root@imx8qmmek:/run/media/mmcblk1p3/videos# gplay-1.0 car.avi
FSL_GPLAY2_01.00_LINUX build on May 20 2019 10:18:11
Set VideoSink imxvideoconvert_g2d ! queue ! waylandsink
Set TextSink fakesink
====== AIUR: 4.4.5 build on May 20 2019 10:17:54. ======
Core: AVI_PARSER_03.06.06 build on Feb 25 2019 02:36:36
file: /usr/lib/imx-mm/parser/lib_avi_parser_arm_elinux.so.3.1
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:06.973633000
Language: und
Mime:
video/mpeg, systemstream=(boolean)false, parsed=(boolean)true, mpegversi
on=(int)4, width=(int)720, height=(int)720, framerate=(fraction)30000/1001, code
c_data=(buffer)000001b001000001b58913000001000000012000c48d8ba98516845a146300000
1b24c61766335372e3130322e313030
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:07.000816000
Language: und
Mime:
audio/mpeg, mpegversion=(int)1, channels=(int)2, rate=(int)44100, bitrat
e=(int)0
------------------------
[ 71.896696] [VPU Decoder] firmware version is 1.3.1
====== BEEP: 4.4.5 build on May 20 2019 10:18:00. ======
Core: MP3 decoder Wrapper build on Jan 11 2018 10:20:25
file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm_elinux.so.3
CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.01_ARMV8 build on Jan 11 2018 10:05:45.
===!!! Current pulsesink device is auto_null !!!===
[Stop (No Repeated)][Vol=1.0][00:00:00/00:00:07]=========== fsl_player_play() ==
================
FSL_GPLAY2_01.00_LINUX build on May 20 2019 10:18:11
[h]display the operation Help
[p]Play
[s]Stop
[e]Seek
[a]Pause when playing, play when paused
[v]Volume
[m]Switch to mute or not
[>]Play next file
[<]Play previous file
[r]Switch to repeated mode or not
[u]Select the video track
[d]Select the audio track
[b]Select the subtitle track
[f]Set full screen
[z]resize the width and height
[t]Rotate
[c]Setting play rate
[i]Display the metadata
[x]eXit
State changed: buffering
State changed: playing
[Playing (No Repeated)][Vol=1.0][00:00:00/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:00/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:00/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:01/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:02/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:03/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:04/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:05/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:06/00:00:07]EOS Found
getNextItem No next item!
No more media file, exit gplay!
State changed: stopped
FSL_PLAYER_UI_MSG_EXIT
Total showed frames (203), playing for (0:00:06.974473000), fps (29.106).
Exit display thread
fsl_player_deinit
Hi zhu
please note that this part is not publicly released yet and not all
features are supported, general steps are provided on
Installing GStreamer on I.MX8QM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------