Seamless redundancy test case failing on LS1028ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Seamless redundancy test case failing on LS1028ARDB

692 Views
jjc1
Contributor II

Hi,

I am trying to test the Seamless redundancy feature in LS1028A RDB, and while running the commands as per the BSPv0.3 document. I always get error saying

tsntool>cbstreamidset --device swp0 --streamhandle 1 --nulldmac 0x7665d268f7d9 --nullvid 1                                                   

Type do not supported!
error streamid type: only null stream identify supported now

Complete log is attached below.

Labels (1)
0 Kudos
2 Replies

485 Views
ufedor
NXP Employee
NXP Employee

The issue will be investigated as Technical Case #00213086

0 Kudos

485 Views
jjc1
Contributor II

I was able to go past this error by adding an additional parameter

--nullstreamid

with the command, but still the test case doesn't work.

Is there anything else missing in document for this test case?

0 Kudos