基于Yocto BSP L4.1.15-2.1.0修改QT5版本

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

基于Yocto BSP L4.1.15-2.1.0修改QT5版本

2,363 Views
1182614726
Contributor III

大家好,

            目前使用的芯片为imx6solo,使用的BSP为Yocto L4.1.15-2.1.0版本。

            目前使用这个版本的BSP编译出来的QT版本为5.6,请问是否可以通过修改Yocto配置文件,生成QT5.5的版本。

            目前暂不想通过升级整个Yocto版本,基于当前Yocto版本修改。

            谢谢。

Labels (1)
0 Kudos
4 Replies

1,878 Views
joanxie
NXP TechSupport
NXP TechSupport

maybe you can try to build qt5.5 to replace it, you need porting by yourself, I send the links for reference

Building Qt5 using yocto on Wandboard - Wandboard Wiki 

https://forum.qt.io/topic/52546/tuto-build-qt-to-cross-compile-for-arm

0 Kudos

785 Views
meifangchang
Contributor I

现在只能升级到5.9.9,能不能升级到5.15

0 Kudos

1,878 Views
1182614726
Contributor III

Hi Joan,

   

         这个帖子Building Qt5 using yocto on Wandboard - Wandboard Wiki提到在yocto/build/conf/bblayers.conf文件增加meta-qt5配置。

         我仔细查看了下我的yocto BSP中的bblayers.conf文件,里面已经包含了meta-qt5。

         另外,这两个帖子的内容与我的问题不太一致。我的yocto BSP中已经配置了meta-qt5,并且qt的版本为5.6.1。我的问题是如何修改将qt从5.6.1版本修改为5.5.1,谢谢支持。

0 Kudos

1,878 Views
joanxie
NXP TechSupport
NXP TechSupport

you can build a similar layer like qt5.6, don't need to remove qt 5.6,

How to downgrade Qt version? 

Ubuntu Forums 

0 Kudos