DDR3L-1066 speed support in SABRE design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3L-1066 speed support in SABRE design

602 Views
talents_titus
Contributor I

I'm currently working on an i.Mx 7D based design, so I use SABRE as my reference. My requirements expect me to include 8Gb DDR3L (Two 4Gb x16 configuration) as per SABRE, but I found that Micron currently doesn't support (backward compatible) DDR3L-1066 4Gb, (referred the DDR3L-2133 datasheet which supports btoth 1866 and 1600). Based on the reference design, SABRE uses DDR3L-1866 (MT41K256M16TW-107:P). So how do they achieve it and is it fine to use the same part or do I need to go with another configuration? Thanks in advance. 

Labels (1)
0 Kudos
2 Replies

486 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Talent Titus,

Most DDR memories are backwards compatible in that they can work on lower clock speeds, just double check on the DDR documentation.

When working on the new DDR setup you may use the i.MX7D DRAM Register Programming Aid:

https://community.nxp.com/docs/DOC-152468

I hope this helps!

Regards,

0 Kudos

486 Views
talents_titus
Contributor I

Thank you for the reply.

0 Kudos