Hi ALL:
I have ever used ddr tools to generate 1G and 2GDDR configure file ddr_init.c and ddrphy_train.c for I.MX8M and works well.
Now I need to configure 3GDDR file ,the ddr tool will calibration and gen code success . but when i make a new imx-boot and burn it into the SD card , it will stuck in kernel stage . the only difference is the DDR size, so, I think the ddr_init.c and ddrphy_train.c may error.
Is there a problem with my configuration?
i will modify follow files on uboot when modify DDR size
board\freescale\imx8mq_evk\ddr\ddr_init.c
board\freescale\imx8mq_evk\ddr\ddrphy_train.c
include\configs\imx8mq_evk.h PHYS_SDRAM_SIZE
We have in place a document that explains how to use the DDR tool, and we have an excel file that help you to select the proper values regarding your memory, here is the link: i.MX8 MSCALE SERIES DDR Tool Release (V2.10)
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------