RGMII with DP83867 in T1022 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RGMII with DP83867 in T1022 board

1,106 Views
hemwant
Contributor IV

We are having a custom board based on T1022 processor having two PHY (DP83867) attached to the processor via RGMII interface. The problem is none of the PHYs are getting detected at uboot using MDC/MDIO interface. We have checked the MDC using scope and it is OK, however there is no transition detected on MDIO line on trying to read through u-boot prompt. I am attaching the uboot log which includes RCW settings of the board.

Any other relevant information needed to debug the issue will be shared. Kindly let us know.

Labels (1)
0 Kudos
3 Replies

783 Views
hemwant
Contributor IV

ufedor‌ Yeah there was some mistake in RCW and phy were available in uboot by changing the RCW settings. Thanks for the reply.

0 Kudos

783 Views
anshulkhare
Contributor III

Hello hemwant@cdot.in

in your Board in LInux kernel RGMII with DP83867 worked??

i am using SDK-V2.0-1701 which has linux kernel 4.1 where i am not getting TI Driver for DP83867

how did you configured RGMII in Linux kernel??

kindly help us to solve this issue.

https://community.nxp.com/thread/498996 

Regards,

Anshul Khare

0 Kudos

783 Views
ufedor
NXP Employee
NXP Employee

1) RCW[EMI1_MODE]=1 - is pull-up for MDIO signal implemented?

2) What is the SCFG_EMIIOCR[MDIO2SEL] value?