I work on a SBC Variscite based on IMX6UL; to replace the second splashscreen I have to compile a .C file using "configure" command.
Some indications about how to cross compile from Linux ? My environment is:
/opt/fslc-x11/2.2.1/environment-setup-armv7at2hf-neon-fslc-linux-gnueabi
Some one could help me?
Hello Paolo Santini,
There is a Hello World example on the following training:
https://community.nxp.com/docs/DOC-95225
There is also an example on this thread’s comments, which is a bit more up to date.
https://community.nxp.com/thread/394804
I hope this helps!
Regards,