IMX6 QUAD support how much capacity for SD card on each port.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 QUAD support how much capacity for SD card on each port.

1,959 Views
matri_manish
Contributor I

I am using imx6 quad # MCIMX6Q6AVT10AD processor. My requirement is to  use 256 GB external micro SD card.

In datasheet , it is not clear will it supoort till 256GB capacity of SD card or not?

If it supports then by using 4-bit or 8-bit data lines and on which uSDHC port, shall i interface?#MCIMX6Q6AVT10AD nxp imx6 imx8 imx-quad#sd card

#imx

Labels (1)
0 Kudos
7 Replies

1,707 Views
igorpadykov
NXP Employee
NXP Employee

Hi matri

one can look at answer on

Maximum External storage(uSD) Capacity Supported by iMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,707 Views
matri_manish
Contributor I

Hi Igor,

Answer is not sufficient, As I read somewhere , it can support till 2TB.

Kindly read my full question and reply back.

0 Kudos

1,707 Views
igorpadykov
NXP Employee
NXP Employee

Hi matri

you are right, SDXC (supported by i.MX6Q) can support up to 2TB:

MultiMediaCard - Wikipedia 

Best regards
igor

0 Kudos

1,707 Views
matri_manish
Contributor I

Hi,

Please let me know on which Usdhc PORT, IT CAN SUPPORT TILL 256GB or interface will be 4-bit or 8-bit data lines.

Please read full question.

0 Kudos

1,707 Views
igorpadykov
NXP Employee
NXP Employee

Hi matri

 

all i.MX6Q uSDHC ports support SDXC, interface width is

described in sect.67.1.1 Features i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

From i.MX6Q there are no restrictions on data width defined by SD specs.

 
Best regards

igor

0 Kudos

1,707 Views
matri_manish
Contributor I

Hi,

Can we directly interface through 4-bit data lines of SD card on USDHC3rd port.?

I have doubt to use 4-bit or 8-bit data lines.

My requirement is to support 256 GB SD card.

Thanks,

Manish

0 Kudos

1,707 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manish

yes it can be connected directly, example can be found in Sabre SD schematic

Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos