imx6ull usdhc2 not working by SDK2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull usdhc2 not working by SDK2

581 Views
alvenwu
Contributor I

I am trying to port the file system including the MMC driver in sdk2 to freertos system.  However , when we use usdhc2  connect to the MMC5.1 chip, we call the MMC_Init to do the initialization. 

the step is 1.after the host initialization , we send CMD0 to reset the bus , seems it works.  here is the function:

 /* Send CMD0 to reset the bus */
    if (kStatus_Success != MMC_GoIdle(card))
    {
        return kStatus_SDMMC_GoIdleFailed;
    }

and after sending a command , it could also enter into interrupt.

but the second command,  it doesnot work. after sending the command , it could not get the response and therefore could enter into interrupt handler, and then keeping waiting for the completion of transfer.

/* Hand-shaking with card to validata the voltage range Host first sending its expected
       information.*/
    if (kStatus_Success != MMC_SendOperationCondition(card, 0U))
    {
        return kStatus_SDMMC_HandShakeOperationConditionFailed;
    }

could anyone give me some indications?  all the code are from official NXP SDK2 package.

0 Kudos
1 Reply

481 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alven

one can check emmc voltages and signals with oscilloscope,

check response from emmc with logic analyzer. Next should be CMD1 command

as described in Figure 22 - e•MMC state diagram eMMC JESD84 specification.
Host issues CMD1 for supported access mode of the memory.

Simple baremetal test can be found in i.MX6Q SDK (1.1.0_iMX6_Platform_SDK.zip)

on link SMP Enable in IMX6 

Also one can test emmc from uboot.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos