Two (and more) SigFox Click elements in one project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two (and more) SigFox Click elements in one project?

741 Views
vilem
Contributor III

Is it possible to have two (or even more) SigFox Click elements in one project? I want to have one to perform periodical tasks and the secon one to be triggered ad hoc (in the case of alert/warning). It is possible to place two SigFox Click elements into NXP Rapid IoT view in the Studio:

twosigfoxes.PNG

Neverteless SigFox Click element is a coupled element with Cloud view. And there is my issue - Only the first instance of SigFox Click element placed to te NXP Rapid IoT view has its mirror created in Cloud view. Does it mean I need to use this element only once?

Labels (1)
0 Kudos
1 Reply

632 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Vilem,

Does it mean I need to use this element only once?

Yes, but you could connect the same element to your 2 tasks that you have. You can achieve this using only one.

Regards,

Mario

0 Kudos