Can Someone give the link for Prebuild (*.sdcard.bz) Imx6 Sabre Sd Board's Linux BSP image. I've been searching for the same for more than 2 days. These are the things which I found
1. L4.1.15_1.0.0_MX6QDPSABRESD
Images provided in both the Links Doesn't seem to work with my board.. all the custom images which i can build is running properly. I wanted to try booting with the pre buiilt default image for the board and check whether a driver is present or not.
Hi Prithvi
right, prebuilt images are specially prepared and built for reference boards
and may not work with custom boards. For custom boards
it is necessary to run ddr test i.MX6/7 DDR Stress Test Tool V3.00
then rebuild images with new calibration coefficients found from ddr test
(put them in uboot/board/..mx6sabresd/mx6q_4x_mt41j128.cfg).
After loading uboot one can try to use rootfs from prebuilt images.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
I'm not using any custom board. I'm using i.MX6QSABRESD https://www.nxp.com/docs/en/user-guide/SABRESDB_IMX6_QSG.pdf
What I'm asking for is that is there any prebuilt images available for the same.. like those which are there for i.MX6QPSABRESD or i.MX6QSOLOX.. etc.
If so, the link for such an image would be appreciated.
Thanks in advance.