I.XM8QXP DDR 校准工具

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.XM8QXP DDR 校准工具

773 Views
ouyangzhiqiang
Contributor II

Dear COMMUNITY:

  Does nxp have a ddr calibration tool that provides im8qxp?I am using IMX8QXP 2GB lpddr4, because there is no ddr calibration tool, so I can't verify it.

2 Replies

451 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Zhiqiang Ouyang,

The calibration works a bit differently for the i.MX8 processors. There is a DDR stress test but there is not a calibration per se. The calibration or DDR training is implemented by the DDR PHY and runs automatically during system boot up.

The stress tool will be very similar to the tool for i.MX8M (link below) and the i.MX8 tool should be available soon after the processor is released.

https://community.nxp.com/docs/DOC-340179

I hope this helps!

Regards,

451 Views
sbertrand
Contributor III

Hi,

Is the DDR tool for iMX8Q series released now ?

I am looking for iMX8QM DDR Tool to perform board validation.

Regards,
Stan

0 Kudos