Is the flash driver for MK64FX512 incorrect?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the flash driver for MK64FX512 incorrect?

Jump to solution
657 Views
yorknh
Contributor IV

Either I am misunderstanding the SRAM available on on an MK64FX512xxx12 or  FTFE_4K.cfx is incorrect. I am using MCUXpresso 10.2.1 and SDK 2.4.2. When I look at the memory settings in the SDK it shows all of the FN variants with 1M of flash and 256K ram. All of the FX variants show 512K of flash and 192K ram. This of course shows up in the MCU settings with the size of SRAM_UPPER only being 0x20000 when I think it should be 0x30000.

0 Kudos
1 Solution
520 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Larry:

Thank you, the page I showed is the reference manual , version 2, 2014. Sorry, I do not update to version 3.

It seems an issue for the SRAM upper size. I have reported this to the software team.

Thanks a lot.

Regards

Daniel

View solution in original post

0 Kudos
3 Replies
520 Views
danielchen
NXP TechSupport
NXP TechSupport

HI Larry

Please refer to the SRAM sizes for the K64 Sub-Family.

For MK64FX512, SRAM_U size is 128 K,  (0x20000)

                             SRAM_L size is 64K.     (0x10000)

pastedImage_1.png

Regards

Daniel

0 Kudos
520 Views
yorknh
Contributor IV

Hi Daniel,

According to Arm® Cortex®-M4|Kinetis® K64 120 MHz 32-bit MCUs|NXP 

and https://community.nxp.com/message/984150?q=k64%20sram 

That page you show is incorrect.

Larry

0 Kudos
521 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Larry:

Thank you, the page I showed is the reference manual , version 2, 2014. Sorry, I do not update to version 3.

It seems an issue for the SRAM upper size. I have reported this to the software team.

Thanks a lot.

Regards

Daniel

0 Kudos