Hardware: MCIMX8M-EVK
Software: 4.9.88_2.0.0
Prebuilt image: fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard.bz2
root@imx8mqevk:~# uname -a
Linux imx8mqevk 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #1 SMP PREEMPT Tue May 1 07:11:12 CDT 2018 aarch64 aarch64 aarch64 GNU/Linux
root@imx8mqevk:~# gst-launch-1.0 videotestsrc ! imxvideoconvert rotation=2 ! ximagesink display=:0
WARNING: erroneous pipeline: no element "imxvideoconvert"
root@imx8mqevk:~# gst-launch-1.0 videotestsrc ! imxvideoconvert_ipu rotation=2 ! ximagesink display=:0
WARNING: erroneous pipeline: no element "imxvideoconvert_ipu"
root@imx8mqevk:~# ls -la /usr/lib/gstreamer-1.0 | grep imxvideoconvert
-rwxr-xr-x 1 root root 48496 May 1 2018 libgstimxvideoconvert.so
root@imx8mqevk:~# gst-inspect-1.0 | grep imx
beep.imx: ac3: ac3
beep.imx: 3ca: ac3
beep.imx: beepdec: Beep universal decoder
aiur.imx: webm: webm
aiur.imx: aiurdemux: Aiur universal demuxer
vpu.imx: vpudec: VPU-based video decoder
Solved! Go to Solution.
Hi Mike
you are right, for i.MX8M such plugins are not available,
p.33 Table 25. i.MX GStreamer 1.0 plugins attached Release Notes
shows available plugins. Also may be helpful to check
https://community.nxp.com/thread/487131
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Mike
you are right, for i.MX8M such plugins are not available,
p.33 Table 25. i.MX GStreamer 1.0 plugins attached Release Notes
shows available plugins. Also may be helpful to check
https://community.nxp.com/thread/487131
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------