i.MX6SoloX 4-Wire Touch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SoloX 4-Wire Touch

383 Views
larrybuccola
Contributor I

Hi All,

I am evaluating the i.MX6SoloXSabreSD board and have my application software running on the SDK build.  I need to interface to a 4-wire resistive touch chip, TSC2046.  Has anyone used a 4-wire resistive touch?  Can anyone point me to a driver that will work on the i.MX6SoloX?

I built a working u-boot/kernel/filesystem using fsl-yocto-L4.9.11_1.0.0.  Any pointers would be greatly appreciated.

Thanks,

Larry

Labels (1)
0 Kudos
1 Reply

308 Views
igorpadykov
NXP Employee
NXP Employee

Hi Larry

for TSC2046 may be useful below

tsc2046 (/ads7846) on imx6 "no irq" problem 

Tweaking Froyo for Nitrogen Part 1: touch support - Boundary Devices 

Configuring i.MX6 boards for different screens - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos