PTB1&PTB0 configured as CAN0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTB1&PTB0 configured as CAN0

665 Views
zhangyan1144
Contributor I

 I configed PTE4 and PTE5 as can0,then the can0 could communicate with can box. But if I configued PTB0 and PTB1 as can0, I modified the relevant code about PTB0 and PTB1, but now the can0 could't send message correctly. I want to know what is the difference between PTE4&PTE5 and PTB0&PTB1 configured as can0.

0 Kudos
2 Replies

543 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Please check this post. The problem is the same and you must check the schematic of the board.

S32K144 FlexCAN0 PTC3/PTC2  Not Working

Best regards,

Razvan

0 Kudos

543 Views
zhangyan1144
Contributor I

Thank you. I didn't use s32k144 EVB to debug can0 configured by PTB1&PTB0. But now I slove this problem.

0 Kudos