Stress test failed on iMX6QP-SDB board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stress test failed on iMX6QP-SDB board

669 Views
lhchang
Contributor I

Hi Sir,

I use attachment to generate a script for DDR test tool on IMX6QP-SDB, but always failed. following is the result. The test always failed on only one uncertain bit. could you please help how to make the stress test successful on the board.

============================================
DDR Stress Test (2.9.2)
Build: Sep 17 2018, 23:07:26
NXP Semiconductors.
============================================

============================================
Chip ID
CHIP ID = i.MX6 Dual/Quad (0x63)
Internal Revision = TO2.0
============================================

============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00000030
SRC_SBMR2(0x020d801c) = 0x12000001
============================================

ARM Clock set to 1GHz

============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 64, bank num: 8
Row size: 14, col size: 10
Chip select CSD0 is used
Density per chip select: 1024MB
============================================


DDR Stress Test Iteration 1
Current Temperature: 35
============================================

DDR Freq: 198 MHz
t0.1: data is addr test
Address of failure(step2): 0x10000000
Data was: 0x00000000
But pattern should match address
Error: failed to run stress test!!!

Labels (1)
0 Kudos
1 Reply

443 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 The DDR Stress tool may be used also for the i.MX6QP with proper initialization script.

 

i.MX6/7 DDR Stress Test Tool V2.92 

 

  I've sent You Aid tools (Excel files) in addition to the published on the Web.

MX6DQP DDR3 Script Aid 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos