i.MX53 BSP with kernel 3.10.17

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 BSP with kernel 3.10.17

1,101 Views
vatsalpatel
Contributor I

Hello All,

I need to work on i.MX53 board and it is required to use kernel 3.10.17. Is there any yocto project setup available for this? If not then is there any alternative?

Thank You,
Vatsal

Labels (2)
0 Kudos
5 Replies

759 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Look at the following:

“Building for i.MX Mature Boards”

 

https://www.nxp.com/docs/en/application-note/AN12024.pdf 

Regards,

Yuri.

0 Kudos

759 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vatsal

unfortunately nxp did not release official bsps for that kernel, in mainline kernels

some proprietary drivers like gpu may be absent. One can also look on

Submit i.MX53 & i.MX28 Linux kernel patches 

https://community.nxp.com/thread/462874 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

759 Views
vatsalpatel
Contributor I

Hello igorpadykov

Thanks for quick reply. Can you please specify which latest kernel and BSP we can use for this board?

Can we use 3.0.35?

What is nxp recommendation for the i.mx53 development?

Best Regards,

Vatsal

0 Kudos

759 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vatsal

if you wish to use gpu, recommended to use latest official bsp L2.6.35_11.09.01:

linux-2.6-imx.git - Freescale i.MX Linux Tree 

L3.0.35 may lack gpu drivers.

 

Best regards
igor

0 Kudos

759 Views
igorpadykov
NXP Employee
NXP Employee

latest official bsp was L2.6.35_11.09.01:

linux-2.6-imx.git - Freescale i.MX Linux Tree 

I am afraid next, including 3.0.35 may lack gpu drivers.

Best regards
igor

0 Kudos