S32K144 MCU "Device is secure, Erase to unsecure"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 MCU "Device is secure, Erase to unsecure"

4,198 Views
香龙朱
Contributor II

When I  debug the CSEc of S32K144, I Use function FLASH_DRV_DEFlashPartition(&flashSSDConfig, 0x02u, 0x08u, 0x03u, false, true). then I Power down and Power up my device.

Now, I can't connect my device via P&E or OpenSDA or J-link.

The S32DS tip me: ”Device is secure,Erase to unsecure“, but I can't Erase my device. S32DS tip me this twice, then S32DS show a disconnect UI to me.

How can I reuse my device via debug tools?

4 Replies

2,964 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can try  Emergency Kinetis device Recovery in debug session settings:

pastedImage_1.png

Jiri

2,964 Views
香龙朱
Contributor II

Hi, Jiri

Thanks for my question.

I have three devices can't be Erased.I tried this method, it is effective on one device. but other two devices have no effect.
I also tried other method. I refer to thread1thread2 and document. I also use script "erase_all_pin.jlk" with j-link.

but I can't erase my other two devices.

I used "unlock kinetis" command, It tips me O.K. but I can't connect my device with J-link or OpenSDA or P&E.

tips-OK.PNG

I used the script "erase_all_pin.jlk", it tips me so many "Protection tip".

tips-protection.PNG

At last it tips me a "Cannot connect to target".

tips-cannot-connect.PNG

There is any other method to reuse my devices?

Thanks a lot.

0 Kudos

2,964 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

your device has probably also disabled mass erase. With this settings there is no way back (device is secured, mass erase disabled). and only soldering iron can solve it. 

Jiri

0 Kudos

2,964 Views
香龙朱
Contributor II

Hi, Jiri

If so, that would be sad.

But,whatever, thank you very much!

Shannon

0 Kudos