Can't find a setting in memuconfig in L4.1.15

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't find a setting in memuconfig in L4.1.15

Jump to solution
1,353 Views
ko-hey
Senior Contributor II

Hi all

 

I'm testing a following thread in SABRE-SD with L4.1.15.

I understand that I have to change a configuration by menuconfig but I can't find a setting in menuconfig window.

https://community.nxp.com/docs/DOC-95014

 

 

Could someone tell me the settings if you know ?

 

 

Ko-hey

 

0 Kudos
1 Solution
1,109 Views
joanxie
NXP TechSupport
NXP TechSupport

you can set .config file directly, the path is <the source code you built>/git, then you use “gedit .config”, you can find all of settings, then you can change what you want to

View solution in original post

0 Kudos
5 Replies
1,109 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the yocto trainig:

https://community.nxp.com/docs/DOC-95045 

0 Kudos
1,112 Views
akifumiokano
NXP Employee
NXP Employee

joanxie, please follow-up kko-hey's question

0 Kudos
1,112 Views
ko-hey
Senior Contributor II

Hi Joan Xie

Thank you for reply.

I know that I can open a configuration window by using following command.

$ bitbake -c menuconfig linux-imx

My question is which do I select in following choices.

Could you tell me that ?

image001.png

Ko-hey

0 Kudos
1,110 Views
joanxie
NXP TechSupport
NXP TechSupport

you can set .config file directly, the path is <the source code you built>/git, then you use “gedit .config”, you can find all of settings, then you can change what you want to

0 Kudos
1,112 Views
ko-hey
Senior Contributor II

Hi joanxie

Could you follow and answer this thread ?

Ko-hey

0 Kudos