How to configure MFGTools on IMX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure MFGTools on IMX7

1,202 Views
864535720
Contributor II

hi:

   I have a board, Its chip model is a MCIMX7D7DVM10SD .

  • I've tried a lot of MFGTools,But it didn't work,and  I saw a post of BBS(mfgtools to imx7d ), which recommended a tool version. When I tried it, there was still no effect. The problem I encountered was how to configure McImx7ddvm10sd,When I changed the model of the chip, as in your manual, "chip = MX6DL Linux Update" changed to"chip = MX7D Linux Update", the tool could not run.

  • pastedImage_18.png
  • pastedImage_19.png
  • pastedImage_20.png
  • I dont change ucl。
Labels (1)
0 Kudos
5 Replies

851 Views
igorpadykov
NXP Employee
NXP Employee

Hi 其东 

for using MCIMX7D7DVM10SD there is no need for changing the model of the chip,

please try to click on appropriate *.vbs file. Check that board USB_OTG_ID signal is high.

Below mfg tool presentation which may be helpful:

AMF-ACC-T1652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

851 Views
864535720
Contributor II

hi igorpadykov

   When I am using MFGTools, should I install the driver of MFGTools first, because after I connect to OTG,My PC did not detect that the device was connected.

  • How do I install the driver

0 Kudos

851 Views
igorpadykov
NXP Employee
NXP Employee

when using MFGTools, windows uses native hid driver when detecting board, so no

need for additional drivers for board.

Best regards
igor

0 Kudos

851 Views
igorpadykov
NXP Employee
NXP Employee

no additional drivers are needed, suggest to

check that board USB_OTG_ID signal is high.

Best regards
igor

0 Kudos

851 Views
864535720
Contributor II

OK,My problem has been solved。

The solution is:把SD卡取下来,然后连接OTG,给开发板上电,这个时候通过MFGTools去查看,会发现开发板是可以识别的,然后再把SD卡给插上去,点击start,就可以开始下载程序。(注意:我的开发板上没有emmc、nand flash等。然后就是我的boot_mode设置其实是没有效果的。为啥没有效果,目前也没有彻底明白。只有问开发板了!)

0 Kudos