Hello,
I'm starting a new project based on MPC5745B, i can't find any code example for this MCU, so i was wondering since it is from the same family as MPC574xG/B/C, does the code examples from these MCU still work on MPC5745B.
Also the application notes documents....
I'm also looking for the mpc5745b.h file that describe the internal registers for the MCU...
Regards,
Hedi
Thanks for your reply,
i took the file MPC5746C.h (Rev 5.0 03-MAY-17) from Example MPC5746C PIT ISR GHS614, it seems that there is a difference between what is in the file and the reference manual (Rev.5 10/2017).
The CAN_Tag type does not have a field named IFLAG3 for the interrupt flags on MB64 to MB95 while the reference Manual describe those fields....
Hi, I could also point out following example codes:
https://www.nxp.com/docs/en/application-note/AN4830.pdf
Also pay attention to MPC5746C/48G comparison:
https://www.nxp.com/docs/en/application-note/AN5114.pdf
MPC5745B is sub-derivative of MPC5746C, also take a look to section 2 Family comparison of device's datasheet:
https://www.nxp.com/docs/en/data-sheet/MPC5746C.pdf
Hi,
Code examples are posted here on community:
https://community.nxp.com/docs/DOC-329623
You can use the MPC5748G examples for this micro without issues.
Peter