Data throughput

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Data throughput

425 Views
eishishibusawa
Contributor III

Dear Sir

 

Customer want to know the throughput when using i.MX6Dual.

There is no data processing in the CPU.

Please consider that there is only data forwarding.

 

Q1.

From PCIe to SATA(SSD).

Is it possible to achieve the throughput more than 100 MB/s?

 

Q2.

How much is the throughput from G-Ethernet to SATA(SSD)?

 

Please let me know if you have any information.

 

Best Regards,

Eishi SHIBUSAWA

Labels (2)
0 Kudos
1 Reply

331 Views
igorpadykov
NXP Employee
NXP Employee

Hi Elshi

1. seems yes, based on throughput data provided on

https://community.nxp.com/docs/DOC-95014 

2. sorry, such data is not available, such hardware were not tested.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos