Is the only source for the iMX6 GPU in the Yocto project?
-> downloads.yoctoproject.org/mirror/sources/imx-gpu-viv-5.0.11.p8.3-hfp.bin
Is there an up-to-date version somewhere? This was from 2016 >< and have long since expired since the xserver uses new ABIs and such.
Here is a reference to the work I've done in so far in implementing the proprietary binaries,
Hi Nate
one can look at latest Linux 4.9.88_2.0.0 BSP, use Yocto Guide for bilding:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Also, why is this assumed answered?!
igorpadykov Thanks for the documentation :-) However, my question was about the most recent location to find these binaries. Obviously, Preferably source code... So where might I find these library files???